Requirement for VDD_SOC_IN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Requirement for VDD_SOC_IN

829件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I'm using HW design checking list rev 3.0 and have question about it.

According to the No.2 of "Power and Decouple" section in schematic tab, there is a following requirement for VDD_SOC_IN.

VDD_SOC_IN requires 66μF of bulk capacitance because it supplies power for both VDD_SOC_CAP and VDD_PU_CAP.

I couldn't find it in datasheet so is this a new requirment for i.MX6 ?

Does the requirement mean that it requires 66uF in total ?

Ko-hey

ラベル(1)
0 件の賞賛
2 返答(返信)

603件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

capacitors values are not defined in datasheet, as they are

chosen based on testing real boards. In attached part of Sabre reference

board schematic spf-27392 there are bulk capacitors (66uF in total)

and several decoupling capacitors (0.22)

spf-27392 p.2.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

603件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thanks!

Ko-hey

0 件の賞賛