Re:enabling Enlightenment in LTIB build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re:enabling Enlightenment in LTIB build

939件の閲覧回数
lily_zhang
NXP Employee
NXP Employee

Hello, Prathamesh:

Glad to see that you are clear for current sitation. You can click "Helpful Answer" or "Correct Answer" for useful answers if you think we can close this topic.

Yes. You can create another thread to discuss GPP (PPP is usually for internal usage). I can help to follow whether there is any other easy way to get GPP packages if anyone is interesting about it.

0 件の賞賛
返信
1 返信

798件の閲覧回数
prathameshghane
Contributor II

@Xiaoli: Creating a branch with relevant title.

Hi all,

I wish to enable Enlightenment support in the BSP. I followed from the above thread that Freescale doesn't provide full support for X11/X-term profiles.Plus, some sources are not present in the GPP (e.g. : libid3tag-0.15.1b.tar.gz)

Is there any way how I can incorporate Enlightenment modules in the LTIB build using minimum profile?

or Can anyone suggest anoy other way to go about this using some entirely different option?

Thanks and regards,

Prathamesh Ghanekar

0 件の賞賛
返信