Re: IMX6Quad Standalone Bare-metal application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: IMX6Quad Standalone Bare-metal application

626 Views
ailtonlopes
Contributor III

I tried to run the SDK and i got this error:


Building power_modes_test [mx6dq smart_device a]
Linking power_modes_test
/home/andersen/Desktop/iMX6_Platform_SDK-master/gcc-arm-none-eabi/bin/arm-none-eabi-ld: cannot find crtbegin.o
/home/andersen/Desktop/iMX6_Platform_SDK-master/gcc-arm-none-eabi/bin/arm-none-eabi-ld: cannot find crti.o
/home/andersen/Desktop/iMX6_Platform_SDK-master/gcc-arm-none-eabi/bin/arm-none-eabi-ld: cannot find crtend.o
/home/andersen/Desktop/iMX6_Platform_SDK-master/gcc-arm-none-eabi/bin/arm-none-eabi-ld: cannot find crtn.o
/home/andersen/Desktop/iMX6_Platform_SDK-master/mk/targets.mk:226: recipe for target '/home/andersen/Desktop/iMX6_Platform_SDK-master/output/mx6dq/power_modes_test/smart_device_rev_a/power_modes_test.elf' failed
make[1]: *** [/home/andersen/Desktop/iMX6_Platform_SDK-master/output/mx6dq/power_modes_test/smart_device_rev_a/power_modes_test.elf] Error 1
Makefile:98: recipe for target 'power_modes_test' failed
make: *** [power_modes_test] Error 2

Build mx6dq smart_device rev_a ALL failed with return code 2!
b45499‌, Yuri, dhaval, Deactivated userigorpadykovDeactivated user


Can you help me solve it?
Thanks for the previous answer,
Kind Regards
Ailton Lopes

0 Kudos
Reply
1 Reply

470 Views
Yuri
NXP Employee
NXP Employee

Hello,

   please check environment settings of Your toolchain.

The  SDK  is  built  using  the  Mentor  Sourcery  CodeBench  Lite  (previously  called  Sourcery  G++  Lite)

version  of  the  arm-­‐none-­‐eabi  GCC  toolchain.  The  full  list  of  CodeBench  Lite  releases  is  available  

on  this  page:

http://www.mentor.com/embedded-software/sourcery-tools/sourcery-codebench/editions/lite-edition/

Download   Linux  installer  package.  The  tarball  packages  do  not  include  all executables.
Install  the  package  under  /opt  or  any  other  local  folder,  and  make  sure  that  the  PATH environment  variable  allows  accessing  these  executables  used  for  the  build  process:  

CC = arm-none-eabi-gcc
CXX = arm-none-eabi-g++
AS = arm-none-eabi-as
AR = arm-none-eabi-ar
LN = arm-none-eabi-ld

Example  (sh  syntax):

$ export PATH=$PATH:<toolchain_install_path>/bin

Source code installation

  The  SDK  source  code  package  can  be  installed  anywhere. It  is  not  recommended  to  use  a  Windows  unzip  program  to  extract  the  sources,  as  this  may result  in  line  endings  being  automatically  converted.  Instead,  the  equivalent  command  of  Linux  should  be  used.

Example:

$ tar zxvf imx6_platform_sdk_v1.1.0.tgz

Build command

  To  build  the  SDK,  use  the   ./tools/build_sdk  command.  
Note:  It  is  important  to  run   build_sdk  from  the  SDK  root  directory,  not  from  within  the
tools directory.

Running make directly

  If you want more control, you can run make directly:

$ make target=mx6dq board=smart_device  boardrev=a test=caam

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply