Hi,
I am using i.MX6 Dualite for one of my design.
The system is turned ON by connecting a switch to the ON_OFF Button of the processor.
What would the impact of not using RTC Crystal in my System in this scenario?
Whether the system Can generate PMIC_ON_REQ signal without 32KHz clock? Note that VDD_SNVS_IN supply is still present in the system.
Thanks and Best Regards,
KP
According to section 60.5 (Power-On Reset and power sequencing) of the
i.MX6(Q) Reference Manual : "The 4ms and 1ms delays are derived from counting the
32kHz RTC clock cycles; the accuracy depends on the accuracy of the RTC. When the
RTC crystal is either absent or in the process of powering up, an internal ring oscillator
will be the source of RTC." So, external RTC clock is not needed for start up.