RT117x EMMC BOOT config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT117x EMMC BOOT config

666 Views
ymj-123
Contributor I

My boad use eMMC 5.1 HS400 standard. I want to change the eMMC boot config for high speed. But when I set HighSpeed mode and 8bit DDR, that will do one success and one fail, show below. Now I change the eFuse BOOT_CFG2[2:1] value 0b'11' 8-bit DDR and BOOT_CFG1[5:4] 0b'1x' High-speed mode. I am worried about sometime RT117x can't boot successfully. And I want to know why 8bit DDR & HighSpeed will cause this.图像_2023-10-13_180251207.png

 

1697191395451.png

 

Labels (1)
0 Kudos
Reply
3 Replies

580 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Is this same issue present on McuBootUtility Tool? I believe that this issue might be related to the eMMC device however it could help to have more details on this issue.

Best regards,
Omar

0 Kudos
Reply

657 Views
ymj-123
Contributor I

I test repower or reset RT117x for many times. It will enter inner boot sometimes and show that it can't boot steady in high speed mode.

0 Kudos
Reply

630 Views
ymj-123
Contributor I

More details, when boot fail, if not use MCUXpresso Secure Provisioning to connet it with serial port, it can boot by self after about 60~70 seconds.

0 Kudos
Reply