RT1176 ENET_1G iperf速度问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1176 ENET_1G iperf速度问题

ソリューションへジャンプ
592件の閲覧回数
1318614689
Contributor II

我使用RT1176EVK的iperf udp例程测试ENET_1G,速度约550MBits/s,这个速度正常吗?

タグ(1)
0 件の賞賛
1 解決策
576件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

These are 1000 Mbps not quite the same but please note that there are also performance differences with the host OS and reported that there were also differences based on the host computer performance that can be significant. Have you tested with other computers and what is the difference?

 

Regards

Daniel

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
577件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

These are 1000 Mbps not quite the same but please note that there are also performance differences with the host OS and reported that there were also differences based on the host computer performance that can be significant. Have you tested with other computers and what is the difference?

 

Regards

Daniel

0 件の賞賛
556件の閲覧回数
1318614689
Contributor II

After changing the network cable and adjusting the iPerf parameter, ENET_1G can run at full speed

0 件の賞賛