RT1176 ENET_1G iperf速度问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 ENET_1G iperf速度问题

Jump to solution
552 Views
1318614689
Contributor II

我使用RT1176EVK的iperf udp例程测试ENET_1G,速度约550MBits/s,这个速度正常吗?

Tags (1)
0 Kudos
1 Solution
536 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

These are 1000 Mbps not quite the same but please note that there are also performance differences with the host OS and reported that there were also differences based on the host computer performance that can be significant. Have you tested with other computers and what is the difference?

 

Regards

Daniel

View solution in original post

0 Kudos
2 Replies
537 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

These are 1000 Mbps not quite the same but please note that there are also performance differences with the host OS and reported that there were also differences based on the host computer performance that can be significant. Have you tested with other computers and what is the difference?

 

Regards

Daniel

0 Kudos
516 Views
1318614689
Contributor II

After changing the network cable and adjusting the iPerf parameter, ENET_1G can run at full speed

0 Kudos