RT1176 .264 video playback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 .264 video playback

446 Views
liangtaotongxue
Contributor I

We use RT1176 to play video in .264 format, and the maximum frame rate for 720p playback is 4Hz. I learned that RT1060 plays 720p with a maximum frame rate of 4Hz, but RT1060 only has 600M main frequency, while RT1176 has 1G main frequency, so I think RT1176 The frame rate of 720p video in .264 format should be greater than 4Hz.

1. Is my conclusion that the 4Hz frame rate is correct, or is my operation wrong?
2. Is it possible that I want to play 720p video at 15Hz frame rate?

0 Kudos
Reply
1 Reply

419 Views
jingpan
NXP TechSupport
NXP TechSupport

HI @liangtaotongxue ,

You can refer to this demo https://github.com/JayHeng/RT-Mp4Player

The performance is as below with the flexram_sdram settings.

 

 

Dest LCD resolution 1280*720

800MHz  RGB888

Src Video

Dec Audio

Dec Video

PXP Conv

CPU loading (25fps)

480*240

0.84

19.589

15.011

51.07%

480*272

0.835

22.168

15.255

57.22%

960*540

0.836

88.633

23.117

100%

1280*720

0.864

143.701ms

24.136ms

100%

 

So, maybe you can lift the framerate by more optimization. But it seems it's really hard to get 15pfs at 1GHz.

 

Regards,

Jing

0 Kudos
Reply