Hello.
If the NVCC_RGMII1 and/or NVCC_RGMII2 pins of iMX6SX can be not powered (some time or totally)?
Best regards,
Vadim Aleynikov
解決済! 解決策の投稿を見る。
Hi Vadim
board design was done when not all documentation was ready,
also for i.MX6SX Table 2-17. Recommended connections for unused analog interfaces
there is no RGMII
http://www.nxp.com/files/32bit/doc/user_guide/IMX6SXHDG.pdf
Best regards
igor
Hi Vadim
board design was done when not all documentation was ready,
also for i.MX6SX Table 2-17. Recommended connections for unused analog interfaces
there is no RGMII
http://www.nxp.com/files/32bit/doc/user_guide/IMX6SXHDG.pdf
Best regards
igor
Thank you Igor very much.
Best regards,
Vadim
Hi Vadim
all power supplies should be provided to processor
with exceptions given in Table 2-21. Recommended connections
for unused analog interfaces i.MX6 System Development User’s Guide
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor.
Thank you for the reply. Table 2-21, which you referred to, contains RGMII. If my understanding is correct, then this means that the RGMII can be left unpowered when it isn't used. Please confirm or correct me.
Best regards,
Vadim
Hi Vadim
Table 2-21 does not show that RGMII can be left unpowered.
It should be powered even not used.
Best regards
igor
Hi Igor.
Unfortunately your answers are not quite clear to me. In the first reply you wrote:
"all power supplies should be provided to processor with exceptions given in Table 2-21"
Table 2-21 contains the RGMII module, but in the next reply you wrote: "Table 2-21 does not show that RGMII can be left unpowered." It seems to me that these statements are not quite consistent.
Does Table 2-21 presents exceptions of the power supplies which must be provided or not?
Then, in the NXP Reference Design schematics ( MCIMX6SX SDB: SPF-27962.pdf), the iMX6SX RGMII modules are supplied by Ethernet PHY chips U18 and U19. And power supplies of U18 and U19 are under software control by signals PERI_PWR_EN and ENET_PWR_EN_B; both these signals are inactive on default. So, on the MCIMX6SX SDB the NVCC_RGMII1 and NVCC_RGMII2 may be not powered totally or at least, they will not be powered all the time depending on the used software.
If this (SPF-27962.pdf) implementation of RGMII and PHY power is correct?
If the iMX6SX RGMII modules can be not powered at least a part of the system operation time?
Best regards,
Vadim