I am relatively new to building my own hardware but I am trying to understand a couple things about this board.
This board has 2 available UART ports and a I2C port from what I can tell.
When installing a Touch Screen the I2C port is populated.
My understanding of the I2C protocol is that it is a buss with multiple device availability for it.
So if I am understanding correctly I should be able to daisy chain multiple I2C devices off this port and they should all work as long as the devices don't share the same ID? I assume the UART is a specialized Serial port.
Also, I seem to be running into this concept that a hobbyist will run into very high costs in building boards.
I am thinking of building a board for myself and I would breadboard most of the work first, then using open source software design a board and make my own board to test out the design. Assuming everything works as intended then I can look at slowly ramping up production if there is interest. It would be a learning experience for me.
Thanks!
Rodney
Solved! Go to Solution.
So 3 I2C can connect 12 devices. If still not enough, you can use the GPIO as an I2C.
One I2C connect 4 devices normally. The experience tell us that the I2C data communication will not stable after connected 5 devices.
Normally, one I2C connect 4 devices and the devices are not the same ID.
Ok, so I really only have 3 I2C ports if I use the LVDS screen since the touch screen takes up 1 I2C address?
I really need to read up more on these to understand them better..
Is the limitation in the protocol or the board its self?
Thank you!
Rodney
So 3 I2C can connect 12 devices. If still not enough, you can use the GPIO as an I2C.
One I2C connect 4 devices normally. The experience tell us that the I2C data communication will not stable after connected 5 devices.