Questions about RT1160's camera interface and software supports status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about RT1160's camera interface and software supports status

ソリューションへジャンプ
1,040件の閲覧回数
Frank_Jianpeng_Zhao
NXP Employee
NXP Employee

Hi,

I have two general questions about RT1160.

1. Can the Parallel Camera Sensor Interface(CSI) and MIPI Camera Interface (MIPI CSI)  be used at same time?  In other words, can the RT1160 support two cameras at once?

2. Regarding software support, what operating systems are already to run on the RT1160, Linux, FreeRTOS...?

BR,

Frank

0 件の賞賛
返信
1 解決策
1,034件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Frank_Jianpeng_Zhao 

    Thanks for your question, just as we talked in the internal TEAMS:

1. Can the Parallel Camera Sensor Interface(CSI) and MIPI Camera Interface (MIPI CSI)  be used at same time?  In other words, can the RT1160 support two cameras at once?

Answer:  MIPI-CSI and parallel CSI can't work at the same time, as the MIPI CSI and parallel CSI at last connect together to the CSI module, so if the customer needs two Camera work at the same time, we suggest one connect MIPI-CSI or parallel CSI, another connect to the flexIO, use the FlexIO simulate it.

This is the flexIO camera application note:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

2. Regarding software support, what operating systems are already to run on the RT1160, Linux, FreeRTOS...?

Answer: Now, RT1160 SDK support the freertos, you can let the customer check the SDK code directly:

https://mcuxpresso.nxp.com/

 

Wish it helps you!

Best Regards,

Kerry

元の投稿で解決策を見る

3 返答(返信)
456件の閲覧回数
bryan_hong
Contributor V

hello @kerryzhou 

Could you share the example for camera ?

I download as below.

bryan_hong_0-1712305853582.png

thanks

Bryan

 

 

Bryan

0 件の賞賛
返信
432件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @bryan_hong ,

 Please check:

SDK_2_15_000_MIMXRT1160-EVK\boards\evkmimxrt1160\driver_examples\csi

 

If you still have question about it, please create your own question post, and let me know.

Best Regards,

Kerry

0 件の賞賛
返信
1,035件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Frank_Jianpeng_Zhao 

    Thanks for your question, just as we talked in the internal TEAMS:

1. Can the Parallel Camera Sensor Interface(CSI) and MIPI Camera Interface (MIPI CSI)  be used at same time?  In other words, can the RT1160 support two cameras at once?

Answer:  MIPI-CSI and parallel CSI can't work at the same time, as the MIPI CSI and parallel CSI at last connect together to the CSI module, so if the customer needs two Camera work at the same time, we suggest one connect MIPI-CSI or parallel CSI, another connect to the flexIO, use the FlexIO simulate it.

This is the flexIO camera application note:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

2. Regarding software support, what operating systems are already to run on the RT1160, Linux, FreeRTOS...?

Answer: Now, RT1160 SDK support the freertos, you can let the customer check the SDK code directly:

https://mcuxpresso.nxp.com/

 

Wish it helps you!

Best Regards,

Kerry