Hello
I apologize for the delay
Those pins are for ETM trace. If you want to use these as trace outputs, you set the IOMUX mode to ALT4 and the corresponding pin will be a trace output.
For example TRACE0: Set MUX_MODE to 4 to make the pin an ETM trace output.
IOMUXC_SW_MUX_CTL_PAD_SAI1_RXD0 field descriptions
You would use this in combination with a debugger that supports ETM trace capture. With this capability, it is possible to see the program execution that leads to the event.
For information on the debug & trace functionality, please see chapter 4 of the RM.
For details on CoreSight, JTAG debug & ETM, please refer to the ARM documentation which is available on the ARM web site.
In general, such information is only needed for developing a debugger. For normal use, it is sufficient to set the I/O mux and optionally any debugger specific settings.
Best Regards,
Diego.
Hello
I apologize for the delay
Those pins are for ETM trace. If you want to use these as trace outputs, you set the IOMUX mode to ALT4 and the corresponding pin will be a trace output.
For example TRACE0: Set MUX_MODE to 4 to make the pin an ETM trace output.
IOMUXC_SW_MUX_CTL_PAD_SAI1_RXD0 field descriptions
You would use this in combination with a debugger that supports ETM trace capture. With this capability, it is possible to see the program execution that leads to the event.
For information on the debug & trace functionality, please see chapter 4 of the RM.
For details on CoreSight, JTAG debug & ETM, please refer to the ARM documentation which is available on the ARM web site.
In general, such information is only needed for developing a debugger. For normal use, it is sufficient to set the I/O mux and optionally any debugger specific settings.
Best Regards,
Diego.