Question, i.MX6Q H.264 encoding with B-Frames

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6Q H.264 encoding with B-Frames

ソリューションへジャンプ
4,159件の閲覧回数
SLICE
Contributor IV

Dear team,

My customer is using i.MX6Q for their system, and they are using  gstreamer for encoding H.264 video.

They are using Linux(L3.0.35_4.0.0_130424 base) as OS.

And once they tried to use B-Frame in H.264 Encoding but it did not get succeed.

Currently, they are using I and P-frames for H.264 encoding.

Could you show me the way to use B-Frames for H.264 encoding?

Is it possible to use B-frames in H.264 encoding on i.MX6Q?

Thanks,

Miyamoto

ラベル(2)
0 件の賞賛
返信
1 解決策
3,837件の閲覧回数
frank_zhang
NXP Employee
NXP Employee

Hi Miyamoto-san,

    Based on i.MX6DQ RM chapter 69.1.1 Features.

    VPU supports H.264 BP/CBP/MP/HP decoding and H.264 BP/CBP encoding.

    We can know the difference between these profiles by the below figure in WIKIH.264/MPEG-4 AVC - Wikipedia 

pastedImage_2.png 

Best Regards,

Frank

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,838件の閲覧回数
frank_zhang
NXP Employee
NXP Employee

Hi Miyamoto-san,

    Based on i.MX6DQ RM chapter 69.1.1 Features.

    VPU supports H.264 BP/CBP/MP/HP decoding and H.264 BP/CBP encoding.

    We can know the difference between these profiles by the below figure in WIKIH.264/MPEG-4 AVC - Wikipedia 

pastedImage_2.png 

Best Regards,

Frank

0 件の賞賛
返信
3,837件の閲覧回数
SLICE
Contributor IV

Hello FrankZhang‌

Thanks for your prompt reply.

Let me clarify my understanding.

The specification of VPU/i.MX6Q is to support H.264 encoding BP and CBP profile.

And the BP/CBP is not using B-Frames.

So, VPU of i.MX6Q does not support using B-Frames in H.264 encoding.

Correct?

Thanks,

Miyamoto

0 件の賞賛
返信
3,837件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the vpu reference manual, encoding doesn't support, but decoding supports it.

0 件の賞賛
返信
3,836件の閲覧回数
frank_zhang
NXP Employee
NXP Employee

Hi Miyamoto-san,

     I think your understanding is correct. Also you can refer to VPU programing guide attached for VPU programing.Thank you. 

Best Regards,

Frank

0 件の賞賛
返信