Dear team,
I would like to ask about ENABLE_DCDC bit setting of i.MX28.
My customer is confused on the setting of ENABLE_DCDC bits.
There are two ENABLE_DCDC bits;
One is in HW_POWER_5VCTRL register and another is in HW_POWER_DCDC4P2 register.
In i.MX28 reference manual, it is said as follows for the description of the bit in HW_POWER_DCDC4P2 register.
“Enable the dcdc converter to use the DCDC_4P2 pin as a power source…”
In my understanding the DCDC_4P2 comes from internal 4P2 LinReg. And it also means 5V is present as reference manual says as the description for the bit in HW_POWER_5VCTRL.
So, the customer thinks the meanings of two ENABLE_DCDC bits are the same.
Could you give a help to better understanding on the two ENABLE_DCDC bits setting?
Thanks,
Miyamoto
解決済! 解決策の投稿を見る。
The DCDC converter has two power sources :
1) VDD5V via the VDD4P2 ;
2) DCDC_BATT input.
HW_POWER_DCDC4P2[ENABLE_DCDC] serves to select the source of the
DCDC converter : DCDC_4P2 or DCDC_BATT.
HW_POWER_5VCTRL bit will cause the DCDC converter
to remain on after 5V (VDD5V) is connected in order to guarantee
stable supply voltage. Please take a look at section 11.3.2.1 (Battery
Power to 5-V Power ) of the i.MX28 Reference Manual.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The DCDC converter has two power sources :
1) VDD5V via the VDD4P2 ;
2) DCDC_BATT input.
HW_POWER_DCDC4P2[ENABLE_DCDC] serves to select the source of the
DCDC converter : DCDC_4P2 or DCDC_BATT.
HW_POWER_5VCTRL bit will cause the DCDC converter
to remain on after 5V (VDD5V) is connected in order to guarantee
stable supply voltage. Please take a look at section 11.3.2.1 (Battery
Power to 5-V Power ) of the i.MX28 Reference Manual.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------