Dear team,
I would like to ask about BT_SPARE_SIZ setting of i.MX25.
On my customer’s i.MX25 board, NAND-flash which has page-size of 512Byte is used for Boot storage.
i.MX25 does not boot-up when they set BT_SPARE_SIZ to 218B.
And when they set BT_SPARE_SIZ to 128B, then i.MX25 can boot-up.
Is setting BT_SPARE_SIZ reasonable for 512B pagesize NAND?
Could you show me what BT_SPARE_SIZ should be set to for 512b pagesize NAND?
And please let me know BT_SPARE_SIZ setting for 2KB NAND as well.
Thanks,
Miyamoto
解決済! 解決策の投稿を見る。
Please refer to Table 3 (Fuse Descriptions) of the app note AN3684, regarding
using the spare size parameter :
BT_SPARE_SIZE - Specifies the size of spare bytes for 4 Kbyte page size NAND
Flash devices.
Note: 512 byte page devices have 16 bytes spare area size,
2 Kbyte page devices have 64 bytes spare area size.
Note: Assumes that the large spare area devices (218 byte) use 8-bit ECC.
Otherwise, 4-bit ECC.
< http://cache.freescale.com/files/dsp/doc/app_note/AN3684.pdf >
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Please refer to Table 3 (Fuse Descriptions) of the app note AN3684, regarding
using the spare size parameter :
BT_SPARE_SIZE - Specifies the size of spare bytes for 4 Kbyte page size NAND
Flash devices.
Note: 512 byte page devices have 16 bytes spare area size,
2 Kbyte page devices have 64 bytes spare area size.
Note: Assumes that the large spare area devices (218 byte) use 8-bit ECC.
Otherwise, 4-bit ECC.
< http://cache.freescale.com/files/dsp/doc/app_note/AN3684.pdf >
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri,
Thanks for your reply.
Can I understand that BT_SPARE_SIZE must be 0(128B) for 512B and 2KB pagesize NAND?
Best Regards,
Miyamoto
Correct - "BT_SPARE_SIZE must be 0(128B) for 512B and 2KB pagesize NAND".
~Yuri.