Hi,
I have query for porting KSZ9031 to imx6sx
Guide:
Query#1: As per above document, mentioned changes are in uboot and kernel level both. Does uboot changes required/must? Does only kernel changes works fine?
Query#2: Above document does not mentioned how many changes to enable in kernel configuration like CONFIG_MICREL_PHY=y. So does only CONFIG_MICREL_PHY enough to detect KSZ9031 phy?
I am getting KSZ9031 is detected as Generic PHY.
"fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:00, irq=-1)"
Any idea for the same?
解決済! 解決策の投稿を見る。
Hi Rakesh
>Query#1:
yes all these changes are needed.
>Query#2:
CONFIG_MICREL_PHY=y adds some specific micrel initializations, like "Pad Skew".
Seems without them it can work fine too, as generic phy. One can try to debug it
also may be recommended to post issue on uboot mail list
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Rakesh
>Query#1:
yes all these changes are needed.
>Query#2:
CONFIG_MICREL_PHY=y adds some specific micrel initializations, like "Pad Skew".
Seems without them it can work fine too, as generic phy. One can try to debug it
also may be recommended to post issue on uboot mail list
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------