Dear all,
I am working with Qt5.5.0 and QtCreator 3.4.2 open source. On the hardware side I work with a i.MX6 sabre platform for smart devices.
As a first aproach, after having created the image fsl-image-qt5 correctly (I think), I would like to run different examples by cross compiling and executing them on the SABRE platform. On my PC I run Ubuntu 14.04 LTS.
When I compile all the examples to run on the Ubuntu PC, they all work properly (bluetooth, qtquick ...)
However, when I try to cross-compile and run them on the SABRE platform, I get execution errors with some of them.
When I try to run a bluetooth scanner, I get:
./btscanner: error while loading shared libraries: libQt5Bluetooth.so.5: cannot open shared object file: No such file or directory
When I try to run a Qtquick example (dasboard), I get:
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
QQmlApplicationEngine failed to load component
qrc:/qml/dashboard.qml:45 module "QtQuick.Extras" is not installed
qrc:/qml/dashboard.qml:43 module "QtQuick.Controls" is not installed
qrc:/qml/dashboard.qml:44 module "QtQuick.Controls.Styles" is not installed
qrc:/qml/dashboard.qml:45 module "QtQuick.Extras" is not installed
qrc:/qml/dashboard.qml:43 module "QtQuick.Controls" is not installed
qrc:/qml/dashboard.qml:44 module "QtQuick.Controls.Styles" is not installed
qrc:/qml/dashboard.qml:45 module "QtQuick.Extras" is not installed
qrc:/qml/dashboard.qml:43 module "QtQuick.Controls" is not installed
qrc:/qml/dashboard.qml:44 module "QtQuick.Controls.Styles" is not installed
Can you please give me any advice on what to do? I am stuck at this point.
thank you in advance!
Regards
Hi LuisCasado
I want Qt5.5 exactly, but build fsl-image-qt5 it's not a Qt5.5. Do you have any other option??
Regards,
Aravinth
Hi,
Which examples are you compiling?
I'd like to test that out. But make sure that the libQt5Bluetooth.so.5 is found in /usr/lib folder.
If it does not exist I would look for it in the sysroot of the host, if found there copy it to the rootfs of the target.
/Alejandro
Hi Alejandro,
I have bin able to execute some more examples.
I guess cross-compilation and SDK installation are OK, but I have some doubts on what to add to the IMAGE with IMAGE_INSTALL
However, when I try to execute dashboard example, I get the error:
root@imx6qsabresd:~/fcm/dashboard# ./dashboard
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
QQmlApplicationEngine failed to load component
qrc:/qml/dashboard.qml:43 module "QtQuick.Controls" version 1.4 is not installed
And when I try to execute planets example, I get the error:
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
qrc:/planets.qml:38:1: module "QtCanvas3D" is not installed
Unable to find an X11 visual which matches EGL config 5
At the moment, this is what I add to the fsl-image-qt5:
IMAGE_INSTALL_append = " python-core \
apache2 \
php \
qtbase-fonts \
qtbase-plugins \
qtbase-tools \
qtbase-examples \
qtdeclarative \
qtdeclarative-plugins \
qtdeclarative-tools \
qtdeclarative-examples \
qtdeclarative-qmlplugins \
qtmultimedia \
qtmultimedia-plugins \
qtmultimedia-examples \
qtmultimedia-qmlplugins \
qtsvg \
qtsvg-plugins \
qtsensors \
qtimageformats-plugins \
qtsystems \
qtsystems-tools \
qtsystems-examples \
qtsystems-qmlplugins \
qtscript \
qt3d \
qt3d-examples \
qt3d-qmlplugins \
qt3d-tools \
qtwebkit \
qtwebkit-examples-examples \
qtwebkit-qmlplugins \
qtgraphicaleffects-qmlplugins \
qtconnectivity-dev \
qtconnectivity-mkspecs \
qtconnectivity-qmlplugins \
qtlocation-plugins \
qtlocation-qmlplugins \
qtquickcontrols-qmlplugins \
qtquick1 \
qtquick1-qmlplugins \
qtquick1-plugins \
i2c-tools \
"
These are the modules that are installed in my board:
root@imx6qsabresd:/usr/lib# ls libQt5*.so
libQt5Bluetooth.so libQt5OpenGL.so libQt5Sql.so
libQt5Concurrent.so libQt5PrintSupport.so libQt5Test.so
libQt5Core.so libQt5Qml.so libQt5Widgets.so
libQt5DBus.so libQt5Quick.so libQt5Xml.so
libQt5Gui.so libQt5QuickParticles.so libQt5XmlPatterns.so
libQt5Network.so libQt5QuickTest.so
libQt5Nfc.so libQt5QuickWidgets.so
Thank you very much for your feedback!