You can easily use Yocto as mentioned by Otavio, but if you'd like to use LTIB or build QT without LTIB or Yocto, you can follow this link:
https://community.freescale.com/message/278112#278112
This link provides a patch to make Freescale Gstreamer plugins work on QT.
Rgds
Rogerio
You can easily use Yocto as mentioned by Otavio, but if you'd like to use LTIB or build QT without LTIB or Yocto, you can follow this link:
https://community.freescale.com/message/278112#278112
This link provides a patch to make Freescale Gstreamer plugins work on QT.
Rgds
Rogerio
This integration is ready for you in Yocto. If you use 'danny' branch you'll get Qt 4.8.1 ready for use.
Please learn more about Yocto at:
http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html
Pardon ,I am not good at English.
I install Qt Embedded 4.7.2 and Qt 4.7.2.
under Qt 4.7.2 environments, I create a project , that project (make embed player video and audio by gstreamer, the window displays other information at the same time . It compile success, run OK, ) . This project needs to add gstreamer lib.such as
CONFIG += link_pkgconfig
PKGCONFIG += gstreamer-0.10 gstreamer-interfaces-0.10
But Qt Embedded 4.7.2 environments, I do not know how to add fsl gstreamer lib to Embedded Qt environments , so the project compile failure. So I want to know how to add gstreamer lib to Qt environments?
For the gstreamer direct use I cannot help, maybe LeonardoSandovalGonzalez knows more about it?
I used Phonon as we integrated the gstreamer plugin onto it, in Yocto.