environment: QT 5.3.2,
LTIB: L3.0.35_4.1.0_130816_source
I can successfully compile QT5.3.2: qt-everywhere-opensource-src-5.3.2 by following the steps mentioned in:
Adeneo Embedded: Building Qt 5.1 for Freescale i.MX6 – A white paper by Cuong Chou .
But I also need QTMultimedia module with a gstreamer as backend.
When I start to build QTMultimedia, I run into error as follows:
make[3]: Entering directory `/home/tyt/project/multimedia/src/plugins/videonode'
cd imx6/ && ( test -e Makefile || /home/tyt/project/build/bin/qmake /home/tyt/project/qt-everywhere-opensource-src-5.3.2/qtmultimedia/src/plugins/videonode/imx6/imx6.pro -o Makefile ) && make -f Makefile
Project ERROR: Unknown module(s) in QT: qtmultimediaquicktools-private
make[3]: *** [sub-imx6-make_first] Error 3
The commands I used are:
1. qmake -o Makefile ../qt-everywhere-opensource-src-5.3.2/qtmultimedia/qtmultimedia.pro
Info: creating cache file /home/tyt/project/multimedia/.qmake.cache
Checking for openal... no
Checking for alsa... yes
Checking for pulseaudio... no
Checking for gstreamer... yes
Checking for gstreamer_photography... no
Checking for gstreamer_encodingprofiles... yes
Checking for gstreamer_appsrc... yes
Checking for linux_v4l... yes
Checking for resourcepolicy... no
Checking for gpu_vivante... yes
2. make
Could somebody help me on this?
Thanks in advance