Hi Qt developers,
I wanted to develop applications using Qt on my custom board with imx233. So, I built Qt 4.7.2 and I was able to run the demos on the target. I have a 3.5" TFT w/resistive 4-wire touch and three push buttons. The push buttons are working, But Qt has no response when the screen is touched.
while building Qt for target I have config options, -mouse-tslib -kbd-tty
the usb port on my board doesn't support host mode, so I can't use mouse or keyboard. The only option I've is to get the touch work.
Please share your experience as to how to enable touch when using Qt.
Ps: my touch screen works great with the FSL gnome release...
Did you do following before running Qt app?
export QWS_MOUSE_PROTO=tslib:/dev/input/event1
export TSLIB_TSDEVICE=/dev/input/event1
(you may have to change event1 to one that you have showing up on i.MX233)