Hi,
I am right in assuming that the demo image that comes with the QSB only supports two resolutions on the LVDS interface?
By looking in ldb.c I can only see references to 1080P60 and XGA, whereas I was looking for support for WVGA. Could I just add the resolution to ldb.c and recompile the kernel and go from there? For the sake of completeness my bootargs are lvds=video=mxcdi0fb:RGB666,XGA ldb.
It's a bit disappoiting that the QSB doesn't support a greater range of screen resolutions out of the box.
Thanks
W
1. The QS demo image assumed to use HanStar LVDS panel.
2. If you want to use different LVDS panel with QS board, you must ensure the LVDS cable and LVDS panel are compatible with MX53 QS board.
3. You can follow some instructions under http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf?fsrch=1&sr=1 for customized LVDS usage.
hi
did you find a solution to the above
thanks
liran