i flash Q10.0.0_2.3.0_DEMO_8Q img to MCIMX8QXP-CPU,but I can't connect to it using adb.
I compile the image generated by Q10.0.0_2.3.0_ANDROID_SOURCE and it will not work.
Do I need to modify anything?
Solved! Go to Solution.
I don't know, I didn't pay attention, I directly started to configure mipi display, and then adb was fine.
Before comparison, i2c-adapter has increased a lot,Looks like M4 started。
Have you install the Android SDK Platform-Tools?
I have installed adb tool。If I use Q10.0.0_2.2.0_AUTO_DEMO_8Q, I can connect to it using adb
Q10.0.0_2.5.0_DEMO_8Q also failed!
What's your steps?
download Q10.0.0_2.3.0_DEMO_8Q ,and Execute .\uuu_imx_android_flash.bat -f imx8qxp。
Boot machine, I cannot use adb to connect to the machine on the computer, and neither of the two usb ports will work.
Which version MCIMX8QXP-CPU board are you using, B0 or C0 version?
Good morning, is there a result?
I am using the official development kit. B0 version
Does it work well on your side? In my board I install the Android SDK Platform-Tools will be OK.
I don't know, I didn't pay attention, I directly started to configure mipi display, and then adb was fine.
Before comparison, i2c-adapter has increased a lot,Looks like M4 started。