Project ERROR: Unknown module(s) in QT: webengine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project ERROR: Unknown module(s) in QT: webengine

2,295件の閲覧回数
charles-chau
Contributor II

I am working on getting QtWebengine (5.5) to work with Wandboard-quad.

So far, I have compiled the framebuffer image with Yocto Jethro to boot up on the wandboard.

Compiling with my Ubuntu 14.04 environment is fine. but when I tried to cross compiled the Quick Nano Browser from Qt Example, Qt gives me an error Project ERROR: Unknown module(s) in QT: webengine

The SDK I used is meta-toolchain-qt5

Do you know whether QtWebengine (5.5) is compatible with Freescale Arm i.mx6? What is happening for the error mentioned above?

0 件の賞賛
1 返信

715件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Charles Chau,

Unfortunately the BSP does not implement Qt WebEngine although I believe some of the libraries are included as part of the Qt image. I would recommend investigating about this module perhaps in Qt forums  as you would need to add this module manually as it’s not supported by the BSP. I cannot think of HW limitations that would stop you from adding this module though.

Regards,

0 件の賞賛