Hi all,
I'm new one to LTIB...
i've followed instructions from some forums and sites to DL & run LTIB..
i've stopped at "wget-ssl" & "rpm build"
*********************************************************
Processing platform: Host support packages
============================================
using /home/jag/Desktop/ltib/config/platform/host/ltib.preconfig
Processing: fake-provides
===========================
Processing: mkspooflinks
==========================
Processing: distcc
====================
Processing: ccache
====================
Processing: bison
===================
Processing: flex
==================
Processing: texinfo
=====================
Processing: autoconf
======================
Processing: libtool
=====================
Processing: lkc
=================
Processing: patch
===================
Processing: wget-ssl
======================
Build path taken because: no prebuilt rpm,
rpmbuild --dbpath ///opt/ltib/var/lib/rpm --target i686 --define '_unpackaged_files_terminate_build 0' --define '_target_cpu i686' --define '__strip strip' --define '_topdir /opt/ltib/usr/src/rpm' --define '_prefix /opt/ltib/usr' --define '_tmppath /home/jag/Desktop/ltib/tmp' --define '_rpmdir /opt/ltib/usr/src/rpm/RPMS' --define '_mandir /opt/ltib/usr/share/man' --define '_sysconfdir /opt/ltib/etc' --define '_localstatedir /var' -bb --clean --rmsource /home/jag/Desktop/ltib/dist/lfs-5.1/wget/wget-ssl.spec
.
.
.
.
.
checking for libgnutls... no
configure: error: --with-ssl was given, but GNUTLS is not available.
error: Bad exit status from /home/jag/Desktop/ltib/tmp/rpm-tmp.13495 (%build)
RPM build errors:
Bad exit status from /home/jag/Desktop/ltib/tmp/rpm-tmp.13495 (%build)
Build time for wget-ssl: 48 seconds
Failed building wget-ssl
Died at ./ltib line 1492.
traceback:
main::build_host_rpms:1492
main::host_checks:1554
main:562
Started: Sun Sep 14 02:07:47 2014
Ended: Sun Sep 14 02:08:35 2014
Elapsed: 48 seconds
VERSION : 13.2.1
CVS_VERSION : $Revision: 1.93 $ (Savannah)
PLATFORM : host
GNUTARCH : i686
TOOLCHAIN :
TOOLCHAIN_CFLAGS :
These packages failed to build:
wget-ssl
Build Failed
*****************************************
I've tried all fixes got from net...
but i'm unable to run LTIB on my PC...
I've installed Ubuntu 10.04 in my VMplayer..
please suggest me solution..
thanQ in advance...!!!!!!
Hi All,
after all I've compiled and run LTIB on my PC..
but this time i got another source from friend, which is 1.3GB tar file,
now i got all required libraries and sources are with in the tar file,
"L3.0.35_4.1.0_130816_source.tar".....
Now no issues in running and using LTIB...
thankyou all.....
Hi jagadeesh,
Which board and BSP are you using?
Have a great day,
(Dan)
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Dan,
for Just now my task is to run LTIB successfully on my PC....
after that i'll use it for iMX6sl...
now is that matter of "BSP"....???
Hi jagadeesh,
No, I mean which version BSP you are using so that I can give you the user guide document. As you have installed the LTIB on your PC, and the next step is to build the BSP using LTIB.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dan,
did you got the correct answer for the BSP version.... ??
i need some help... urgent..
I've installed LTIB .. following these instructions from the below link....
and installed the required packages...
thanks in advance...!!
hi Dan,
my ubuntu configuration ....
jag@ubuntu:~$ uname -a
Linux ubuntu 2.6.32-66-generic #132-Ubuntu SMP Mon Sep 1 18:36:19 UTC 2014 i686 GNU/Linux
jag@ubuntu:~$
thanks in advance...
Hello,
Check this links :
http://importgeek.wordpress.com/
https://community.freescale.com/thread/330319
Regards,
Luis
Hi Luis Casado...
I've followed the above two links...
and installed all patches suggested by them...
after running LTIB a got this log....
*******************************************
Processing platform: Host support packages
============================================
using /home/jag/Desktop/ltib/config/platform/host/ltib.preconfig
Processing: fake-provides
===========================
Processing: mkspooflinks
==========================
Processing: distcc
====================
Processing: ccache
====================
Processing: bison
===================
Processing: flex
==================
Processing: texinfo
=====================
Processing: autoconf
======================
Processing: libtool
=====================
Processing: lkc
=================
Processing: patch
===================
Processing: wget-ssl
======================
Build path taken because: no prebuilt rpm,
Use of uninitialized value in string eq at /home/jag/Desktop/ltib/bin/Ltibutils.pm line 370.
Try wget-1.14-perl5.18-fix.patch.md5 from the GPP
http://bitshrine.org/gpp//wget-1.14-perl5.18-fix.patch.md5:
2014-09-15 08:59:36 ERROR 404: Not Found.
Use of uninitialized value in string eq at /home/jag/Desktop/ltib/bin/Ltibutils.pm line 370.
Try wget-1.14-perl5.18-fix.patch from the GPP
http://bitshrine.org/gpp//wget-1.14-perl5.18-fix.patch:
2014-09-15 08:59:37 ERROR 404: Not Found.
Can't get: wget-1.14-perl5.18-fix.patch at ./ltib line 790.
Died at ./ltib line 1380.
traceback:
main::build_host_rpms:1380
main::host_checks:1435
main:542
Started: Mon Sep 15 08:59:35 2014
Ended: Mon Sep 15 08:59:37 2014
Elapsed: 2 seconds
These packages failed to build:
wget-ssl
Build Failed
*******************************************
for wget-ssl building error... all are suggested that .." include --without-ssl " in ./config line in this path dist/lfs-5.1/wget/wget.spec
but this is already exist... in that line..
I'm unable to run this....
thanQ.. n suggest me how to build correctly...
Your build fails because some packages are not found in bitshrine.org
ERROR 404: Not Found.
But I don't know why that patch should be needed, as LTIB builds wget-1.9.1.tar.gz that you should have in /opt/Freescale/pkgs
What is the BSP you're installing?
Luis
Hi Luis,
previously... I run some scripts from some other forum... so i got them..
now i've cleared all those things and run the LTIB again...
i got struced again in processing wget-ssl...
the log is here..
***************************************************
Processing platform: Host support packages
============================================
using /home/jag/Desktop/ltib/config/platform/host/ltib.preconfig
Processing: fake-provides
===========================
Processing: mkspooflinks
==========================
Processing: distcc
====================
Processing: ccache
====================
Processing: bison
===================
Processing: flex
==================
Processing: texinfo
=====================
Processing: autoconf
======================
Processing: libtool
=====================
Processing: lkc
=================
Processing: patch
===================
Processing: wget-ssl
======================
Build path taken because: directory build, no prebuilt rpm,
Cowardly refusing to clobber existing directory:
/opt/ltib/usr/src/rpm/BUILD/wget-1.14
Remove this by hand if you really want to rebuild this package from scratch
Died at ./ltib line 1492.
traceback:
main::build_host_rpms:1492
main::host_checks:1554
main:562
Started: Sat Sep 27 10:35:30 2014
Ended: Sat Sep 27 10:35:30 2014
Elapsed: 0 seconds
VERSION : 13.2.1
CVS_VERSION : $Revision: 1.93 $ (Savannah)
PLATFORM : host
GNUTARCH : i686
TOOLCHAIN :
TOOLCHAIN_CFLAGS :
These packages failed to build:
wget-ssl
Build Failed
***************************************************
i'm new one to the LTIB and want run LTIB on my PC (UBUNTU 10.04)...
if I pass in that i'll get work for iMX6SL......
so please help me to set this....
got this log after removing wget.spec..
.
.
.
.
checking for compress in -lz... (cached) yes
checking for gpg_err_init in -lgpg-error... no
checking for gcry_control in -lgcrypt... no
checking for libgnutls... no
configure: error: --with-ssl was given, but GNUTLS is not available.
error: Bad exit status from /home/jag/Desktop/ltib/tmp/rpm-tmp.87523 (%build)
RPM build errors:
Bad exit status from /home/jag/Desktop/ltib/tmp/rpm-tmp.87523 (%build)
Build time for wget-ssl: 37 seconds
Failed building wget-ssl
Died at ./ltib line 1492.
traceback:
main::build_host_rpms:1492
main::host_checks:1554
main:562
Started: Sat Sep 27 10:46:20 2014
Ended: Sat Sep 27 10:46:57 2014
Elapsed: 37 seconds
VERSION : 13.2.1
CVS_VERSION : $Revision: 1.93 $ (Savannah)
PLATFORM : host
GNUTARCH : i686
TOOLCHAIN :
TOOLCHAIN_CFLAGS :
These packages failed to build:
wget-ssl
Build Failed
***************************
please help me to fix this....
thanks in advance..