Dear Sir or Madam,
Hello.
BSP: L3.10.17_1.0.0
I'd like to execute the preview function with 720p@60fps from Parallel camera (ov5642) to LVDS or HDMI display on i.MX6Q SABRE-SDP.
[Flow: Camera (OV5642) 720p@60fps --> CSI --> DDR3 --> HDMI or LDB 720p@60fps]
Anr, I tried to below commands.
----
$ modprobe ov5642_camera
$ modprobe mxc_v4l2_capture
$ gst-launch -v mfw_v4lsrc device=/dev/video0 fps-n=60 capture-mode=4 ! mfw_v4lsink disp-width=1280 disp-height=720 motion=2
----
The preview image was possible to display on LVDS or HDMI display.
But, the render fps was 29.953.
Refer to below log.
==========
Interrupt: Stopping pipeline ...
Execution ended after 6008930001 ns.
Setting pipeline to PAUSED ...
Running time 0:00:06.009320000 render fps 29.953
Setting pipeline to READY ...
/GstPipeline:pipeline0/MFW_GST_V4LSINK_INFO_T:mfw_gst_v4lsink_info_t0.GstPad:sink: caps = NULL
/GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0.GstPad:src: caps = NULL
Setting pipeline to NULL ...
Total rendered:180
Freeing pipeline ...
[--->FINALIZE v4l_sink
==========
[Question]
Could you tell me the way of preview 720p@60fps from Parallel camera?
Best Regards,
Keita
Hi,
I am looking to purchase a sabre board for smart devices could you tell me if the board you are using is the SABRE Platform for Smart Devices Based on the|Freescale . If yes does the board come with the MIPI and parallel cameras? If the board does not come with cameras can you tell me what modules you purchased ?
Thank you
Gopal
Hi Gopal,
Thank you for you reply.
I purchased the MCIMX6Q-SDP (SABRE Platform for Smart Devices Based on the i.MX 6 Series).
So, two cameras (Parallel & MIPI) mounted on the MCIMX6Q-SDP.
Keita
Hi Keita,
Thank you for your email.
Best Wishes
Gopal
On Thu, Sep 4, 2014 at 8:16 PM, Keita Nagashima <