Power off Panel Power while deep Sleep mode - iMX6.Q7A-551Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power off Panel Power while deep Sleep mode - iMX6.Q7A-551Board

1,142件の閲覧回数
mauriciorodrigu
Contributor II

Our vending machine is on it's way to have a full working prototype. After some work on deep sleep we were able to put it down to 150mA consumption in deep sleep mode. Wich is quit good, but we discover that If we turn of the power from lcd panel and from touch screen we could even reduce more 40% of the total power in deep sleep mode.

As you can see in the image attached if we remove jumper from JP5 and JP3 we can reduce consumption while in deep sleep in 60 mA. 40% reduction.

While in deep sleep mode shouldn't the panel and touchscreen be completely turned off?

We thought about adding a "intelligent" jumper like switch, to turn it off while in sleep and turn it on when in normal usage. What do you think about this approach to reduce power consumption in deep sleep?

Thanks ind advance for any help or hint.

ラベル(4)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

919件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mauricio

processor can turn off power from external peripherals

in low power mode, it can be done in software. By default

processor does not perform that. Also some processor power supplies

can be lowered or turned off, but most of them are not turned off completely.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

919件の閲覧回数
mauriciorodrigu
Contributor II

Thanks Igorpadykov .That's what I thought . I will contact the manufacturer see if can do something about it. Because this shouldn't be done at application level but at processor level when it's entering low power mode.

0 件の賞賛
返信