Porting KSZ9031RN to imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting KSZ9031RN to imx6

Jump to solution
1,582 Views
bastien
Contributor I

Hello !

I am working on imx6 processor custom board, i added the KSZ9031 phy Ethernet on the board.

Recommendations in the post Porting KSZ9031 to i.MX BSP gives the phy side schematic only.

I am not sure if i correctly connected the RGMII_INT pin (p38) to the imx6 (see attached pictures).

Thank you

BR

 

0 Kudos
Reply
1 Solution
1,567 Views
jimmychan
NXP TechSupport
NXP TechSupport

I use this PHY in a i.MX7D board design. I connected this INT pin to a gpio in case we may check the INT output signal in future. For normal using, we don't need to care this INT signal.

 

pin.png

View solution in original post

0 Kudos
Reply
1 Reply
1,568 Views
jimmychan
NXP TechSupport
NXP TechSupport

I use this PHY in a i.MX7D board design. I connected this INT pin to a gpio in case we may check the INT output signal in future. For normal using, we don't need to care this INT signal.

 

pin.png

0 Kudos
Reply