Hi, All
our custom product is refer to i.MX6Q SABRE and the only modification is the wifi module, ours is AMPAK's AP6335 , we are porting this module to Android 5.1 which use 3.14.52 kernel.
According to the the wifi user guide :
Power control and SDIO card detection
Fill WL_REG_ON GPIO pin number and implement card detection function to dhd_gpio.c as
following:
void bcm_wlan_power_on(int flag)
{
if (flag == 1) {
printk("======== PULL WL_REG_ON HIGH! ========\n");
gpio_set_value(WIFI_WL_REG_ON, 1);
mdelay(100);
printk("======== Card detection to detect SDIO card ========\n");
imx_wifi_mmc_safe_detect(1);
} else {
printk("======== PULL WL_REG_ON HIGH! (flag = %d) ========\n", flag);
gpio_set_value(WIFI_WL_REG_ON, 1);
}
}
when we ported this wifi module to Android 4.3 which use 3.0.35 kernel,the card detect function we used is
int imx_wifi_mmc_safe_detect(int online);
which is located in drivers/mmc/host/sdhci-esdhc-imx.c:827:int imx_wifi_mmc_safe_detect(int online)
drivers/mmc/host/sdhci-esdhc-imx.c:905:EXPORT_SYMBOL(imx_wifi_mmc_safe_detect);
but we just can't find this function anymore in 3.14.52 kernel .
the question is :which function is the card detect function in 3.14.52 kernel ?
Hope for your help!
Regards,
解決済! 解決策の投稿を見る。
Hi li
it is wifi_card_detect(void) in linux/drivers/mmc/host/sdhci-esdhc-imx.c,
also please check attached Chapter 33 MMC/SD/SDIO Host Driver
Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi li
it is wifi_card_detect(void) in linux/drivers/mmc/host/sdhci-esdhc-imx.c,
also please check attached Chapter 33 MMC/SD/SDIO Host Driver
Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor
Thanks for your help.
After reading the Chapter 33 MMC/SD/SDIO Host Driver in Linux Manual,I have found that function (wifi_card_detect(void))in linux/drivers/mmc/host/sdhci-esdhc-imx.c and add it to my driver code ,it compile ok.
when i use insmod command to load ther driver , I got the following information :
insmod system/lib/modules/cfg80211.ko
cfg80211: Calling CRDA to update world regulatory domain
insmod system/lib/modules/bcmdhd.ko <
dhd_module_init: in
======== bcm_wlan_set_plat_data ========
GPIO(WL_HOST_WAKE) = GPIO_4_25
host_oob_irq: 281
host_oob_irq_flags=4
dhd_wifi_platform_load: Enter
Power-up adapter 'DHD generic adapter'
wifi_platform_set_power = 1
======== PULL WL_REG_ON HIGH! ========
======== Card detection to detect SDIO card ========
wifi_platform_bus_enumerate device present 1
failed to power up DHD generic adapter, 3 retry left
wifi_platform_set_power = 0
======== PULL WL_REG_ON LOW! ========
wifi_platform_bus_enumerate device present 0
wifi_platform_set_power = 1
======== PULL WL_REG_ON HIGH! ========
======== Card detection to detect SDIO card ========
wifi_platform_bus_enumerate device present 1
failed to power up DHD generic adapter, 2 retry left
wifi_platform_set_power = 0
======== PULL WL_REG_ON LOW! ========
wifi_platform_bus_enumerate device present 0
wifi_platform_set_power = 1
======== PULL WL_REG_ON HIGH! ========
... ...
======== PULL WL_REG_ON LOW! ========
wifi_platform_bus_enumerate device present 0
failed to power up DHD generic adapter, max retry reached**
unregister wifi platform drivers
wifi_platform_bus_enumerate device present 0
dhd_module_init: Failed to load the driver, try cnt 0
dhd_module_init: Failed to load driver max retry reached**
dhd_module_init: Exit err=-19
I wonder if the WiFi driver I used is too old to run properly on 3.14.52 kernel , I will attach it below ,about this driver ,the file I modified is dhd_gpio.c.can you look at it and see if the changes I made is right .
Thank you again for you time on this case.
Best regards!
li chen.