Plymouth is enabled but its not refelecting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Plymouth is enabled but its not refelecting

1,815 Views
ashoksowndar
Contributor II

Hi,

I have enabled plymouth and dracut packages in my i.MX8M Yocto BSP (b2qt-embedded-qt5-image), with that I have also added a "quiet splash" in the kernel command line (/proc/cmdline). [ With reference to the following link : plymouth/dracut and i.mx6 ]

Note: Please find the screenshot in the attachment

Regards,

Ashok

Tags (2)
0 Kudos
Reply
2 Replies

1,677 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Ashok,

Plymouth recipe is available on the Yocto BSP as part of the OpenEmebedded layer.

http://layers.openembedded.org/layerindex/recipe/39966/

 

I would recommend you looking at the Plymouth homepage:

https://www.freedesktop.org/wiki/Software/Plymouth/

 

There are a couple of resources there that may be of help. As you dragcut there are some commands and more information on the dragcut documentation:

https://mirrors.edge.kernel.org/pub/linux/utils/boot/dracut/dracut.html#_dracut_8

Regards

0 Kudos
Reply

1,677 Views
ashoksowndar
Contributor II

Hi Bio_TICFSL,

I have gone through all the resource mentioned, and tried all the possibilites but results are same. I have no clue where I am missing. 

Can you please provide clear procedure how plymouth to be added in yocto with configuration need to done initramfs and kernel command line.

Regards,

Ashok

0 Kudos
Reply