Pins Tool v6 without internet connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pins Tool v6 without internet connection

1,798件の閲覧回数
anon-696f160ab2
Senior Contributor I

Since v6 there is a different behaviour with the update process compared to v5. v6 cant be used within our network as a because of the tool changes along with our companny restrictions. v5 worked well.

In v6 and windows 7 before using the tool with no admin permissions, the tool has to be updated ones with admin permissions, than the cached data can be used to open/save new cpu-profiles.

In v6 and windows 10 iam not able to start a new design because no CPU-profile can be loaded.

pastedImage_1.png 

ラベル(2)
0 件の賞賛
7 返答(返信)

1,471件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Martin Stelter,

There are a couple of alternatives, one would be connecting to the internet temporarily on another network and downloading the required processor data. Another would be downloading them on a different computer with the Pins Tool and Internet access and exporting the data so that it can be imported on the computer without internet access.

You can see how to do this on the Pins Tool User Guide (link below)

https://www.nxp.com/docs/en/user-guide/IMXPINSGSUG.pdf

If neither of these options are feasible you may open a case requesting this information so that the processor information can be exported and sent to you.

My apologies for the inconvenience. I hope this helps!

Regards,

0 件の賞賛

1,471件の閲覧回数
anon-696f160ab2
Senior Contributor I

gusarambula

That sounds like a workarround for me. To clarify, i see an issue in v6 handling internet connection based on proxy. Maybe proxy seetings are not used correctly in v6.

I wish someone can look into v6 and fix it.

0 件の賞賛

1,471件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Martin Stelter,

I have made an inquiry regarding the repository and proxy settings for the Pins Tool V6. I will let you know as soon as I have more information.

Regards,

0 件の賞賛

1,471件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Martin Stelter,

The reply we received is that there is no difference between v6 and v5 in how the online data download is handled. We'll check with them if Windows10 as OS can have any impact.

Regards,

0 件の賞賛

1,471件の閲覧回数
anon-696f160ab2
Senior Contributor I

Yes please do so. As descriped here there are more customer with the issue: https://community.nxp.com/thread/465340 

0 件の賞賛

1,471件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Martin Stelter,

A similar issue has been encountered previously and in order to fix it a change it <install-dir>/bin/tools.ini is needed, from:

-Dcom.nxp.restapi.server=https://mcuxpresso.nxp.com

To:

-Dcom.nxp.restapi.server=http://mcuxpresso.nxp.com

If this does not solve the issue, would you please share the logs from C:\Users\<username>\.nxp\swtools.log?

Regards,

0 件の賞賛

1,471件の閲覧回数
anon-696f160ab2
Senior Contributor I

Yes this works. I tested with the new version v7.

Will this be implemented in a new version so we dont need to change this manually?

0 件の賞賛