Peer to peer connection using broadr reach

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Peer to peer connection using broadr reach

921件の閲覧回数
ajayvenkatakris
Contributor II

Hi,

   I have two imx6 sabre AI boards with each supporting a BroadR reach PHY card. I have a peer to peer connection in between the boards. I have set up an ip address for both the boards, but while trying to ping between the boards, it says that the network is unreachable. The same set up has worked for the Atheros ENET phy Card. How do I set up the peer to peer connection between the two boards using broadr reach. Both the boards are running linaro Ubuntu.

Thanks,

Ajay Venkatakrishnan

0 件の賞賛
4 返答(返信)

782件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ajay

please create service request to obtain additional patch

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

782件の閲覧回数
ajayvenkatakris
Contributor II

Hi,

    What is patch required for?

Thank you,

Ajay V

0 件の賞賛

782件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one board should be flashed with master (#define BCM89810_MASTER)
image and the other as slave image. Patch provides necessary definitions.

~igor

0 件の賞賛

782件の閲覧回数
ajayvenkatakris
Contributor II

Hi,

    I have created the service request. Kindly provide the required patches and kindly mention how I can apply these patches? Also can I apply these patches for Linaro(Ubuntu) or only for Yocto?

0 件の賞賛