As requested in the following thread, I have created an account with my company email. Would it be possible to receive the parameters to set the pixel clock to 83500000 as discussed in the thread?
Thanks.
解決済! 解決策の投稿を見る。
try add the blow parameters in the samsung_phy_pll_cfg table
Pixel Clock (MHz) |
||
APB | Read / Write |
83.5 |
8 | ||
04 | R/W | D1 |
08 | R/W | 60 |
0C | R/W | 58 |
10 | R/W | 8D |
14 | R/W | 06 |
18 | R/W | 00 |
1C | R/W | 40 |
20 | R/W | 4F |
24 | R/W | 30 |
28 | R/W | 33 |
2C | R/W | 65 |
30 | R/W | 10 |
34 | R/W | A0 |
38 | R/W | 24 |
3C | R/W | 80 |
40 | R/W | 6C |
44 | R/W | F2 |
48 | R/W | 67 |
4C | R/W | 00 |
50 | R/W | 10 |
54 | R/W | 85 |
58 | R/W | 30 |
5C | R/W | 3A |
60 | R/W | 74 |
64 | R/W | 8F |
68 | R/W | 00 |
6C | R/W | 00 |
70 | R/W | 08 |
74 | R/W | 00 |
78 | R/W | 00 |
7C | R/W | 00 |
80 | R/W | 00 |
84 | R/W | 80 |
8C | R/W | 00 |
90 | R/W | 00 |
94 | R/W | 00 |
98 | R/W | 00 |
9C | R/W | 00 |
A0 | R/W | 00 |
A4 | R/W | E0 |
A8 | R/W | 83 |
AC | R/W | 0F |
B0 | R/W | 3E |
B4 | R/W | F8 |
BC | R/W | 00 |
For my HDMI screen, I used the parameter by modetest.
edid information : resolution is 1920x720 , clock is 115.2MHZ , could you provide me with the pll parameters please?
do you mind creating a new case for me?
Hello @joanxie , for my HDMI screen, I need a 51.2Mhz clock, could you provide me with the pll parameters please?
Thank you!
try add the blow parameters in the samsung_phy_pll_cfg table
Pixel Clock (MHz) |
||
APB | Read / Write |
83.5 |
8 | ||
04 | R/W | D1 |
08 | R/W | 60 |
0C | R/W | 58 |
10 | R/W | 8D |
14 | R/W | 06 |
18 | R/W | 00 |
1C | R/W | 40 |
20 | R/W | 4F |
24 | R/W | 30 |
28 | R/W | 33 |
2C | R/W | 65 |
30 | R/W | 10 |
34 | R/W | A0 |
38 | R/W | 24 |
3C | R/W | 80 |
40 | R/W | 6C |
44 | R/W | F2 |
48 | R/W | 67 |
4C | R/W | 00 |
50 | R/W | 10 |
54 | R/W | 85 |
58 | R/W | 30 |
5C | R/W | 3A |
60 | R/W | 74 |
64 | R/W | 8F |
68 | R/W | 00 |
6C | R/W | 00 |
70 | R/W | 08 |
74 | R/W | 00 |
78 | R/W | 00 |
7C | R/W | 00 |
80 | R/W | 00 |
84 | R/W | 80 |
8C | R/W | 00 |
90 | R/W | 00 |
94 | R/W | 00 |
98 | R/W | 00 |
9C | R/W | 00 |
A0 | R/W | 00 |
A4 | R/W | E0 |
A8 | R/W | 83 |
AC | R/W | 0F |
B0 | R/W | 3E |
B4 | R/W | F8 |
BC | R/W | 00 |