Hi all
Does someone have thermal characteristics data for i.MX27 ?
I want a data which likes table 16 of IMX25AEC.pdf for calculation.
Ko-hey
解決済! 解決策の投稿を見る。
as Tj (junction temperature), R (thermal resistance, that may be needed for thermal estimations are not provided. Also thermal parameters are not specified, but they are taken into account implicitly. max Tj = max Ta + R * Pd, where Tj - junction temperature ; Ta - ambient temperature from the datasheet ; R - thermal resistance ; Pd - power dissipation in package. For i.MX27 production technology the junction temperature is ~105C.
Hi Joan Xie
Let me confirm one more thing.
What is the junction temperature for i.MX27 ?
The datasheet shows only temperature like below.
So I can't clarify whether the temperature is junction temperature or not.
Furthermore, according to the following product selector, it shows ambient operating temperature.
As a result, the temperature which shows in table 1 of datasheet isn't junction temperature.
So please tell me the junction temperature for i.MX27.
Ko-hey
Could someone follow and support this question ?
Ko-hey
as Tj (junction temperature), R (thermal resistance, that may be needed for thermal estimations are not provided. Also thermal parameters are not specified, but they are taken into account implicitly. max Tj = max Ta + R * Pd, where Tj - junction temperature ; Ta - ambient temperature from the datasheet ; R - thermal resistance ; Pd - power dissipation in package. For i.MX27 production technology the junction temperature is ~105C.