PWM of IMX6SX cannot be generated continuously

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PWM of IMX6SX cannot be generated continuously

跳至解决方案
572 次查看
longh
Contributor III

Hi All,

   I am working on

pwm changes randomly 

0 项奖励
1 解答
546 次查看
igorpadykov
NXP Employee
NXP Employee

Hi long

if PWM cannot be generated continuously one can check

if it is disabled in low power modes, bits DOZEN, STOPEN, WAITEN

described in sect.49.7.1 PWM Control Register (PWMx_PWMCR)

i.MX 6SoloX Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
547 次查看
igorpadykov
NXP Employee
NXP Employee

Hi long

if PWM cannot be generated continuously one can check

if it is disabled in low power modes, bits DOZEN, STOPEN, WAITEN

described in sect.49.7.1 PWM Control Register (PWMx_PWMCR)

i.MX 6SoloX Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励