PWM of IMX6SX cannot be generated continuously

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM of IMX6SX cannot be generated continuously

ソリューションへジャンプ
1,232件の閲覧回数
longh
Contributor III

Hi All,

   I am working on

pwm changes randomly 

0 件の賞賛
返信
1 解決策
1,206件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi long

if PWM cannot be generated continuously one can check

if it is disabled in low power modes, bits DOZEN, STOPEN, WAITEN

described in sect.49.7.1 PWM Control Register (PWMx_PWMCR)

i.MX 6SoloX Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,207件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi long

if PWM cannot be generated continuously one can check

if it is disabled in low power modes, bits DOZEN, STOPEN, WAITEN

described in sect.49.7.1 PWM Control Register (PWMx_PWMCR)

i.MX 6SoloX Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信