PWM audio for imx6ul

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM audio for imx6ul

5,457 Views
sankarsalla
Contributor II

Hi All,

We are working on playing some .wav files by using pwm.

We found some driver like pwm-beeper.c.

using that driver can i play some .wave files ?

Or we need to develop any other driver for pwm audio,please give me some inputs.

Thanks & Regards,

Sankar.

Labels (1)
Tags (1)
0 Kudos
Reply
17 Replies

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

 

Pwm audio is working fine,but some noise came.

Thanks for your support.

Thanks & Regards,

Sankar.

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

Yes,we are using 1.5k only.

We are using 1W and 8Ohm speaker,full noise coming from speaker.

 

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

Thanks for sharing valuable information.

Actually our requirement is play some raw files through pwm out.

So,if possible can you help us to some check points for exact problem(from speaker full noise is coming) its either driver or circuit?

Same driver is working fine from your end or you modified the driver for playing wav files.

We cross verified the registers of the imx6ul and imx6ull datasheets,both are using same registers and working functionality also same.

Thanks & Regards,

Sankar.

0 Kudos
Reply

4,426 Views
Sasamy
Contributor IV

Hi Sankar.

We use the same driver and filter, but I would like to clarify - the nominal value of resistors r15, r17, r19 is 1.5 kOhm, it's hard to see in the screenshot.

Alexander

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

We are also playing 16 bit,8 bit  and 8KHz .wav files.

PWM pin generates 7.84 KHz from driver,but noise is coming with amplifier and with your suggested circuit noting is coming form speaker.

Something we have to modify in driver or same driver will work ?

can you please help us where we are wrong,actually we are struck in pwm audio.

Thanks & Regards,

Sankar.

   

0 Kudos
Reply

4,426 Views
Sasamy
Contributor IV

Hi Sankar.

The use of conventional PWM is an alternative solution and I agree with Igor - it is better to use SAI + MQS because they have many advantages

1 support DMA out of the box
2 multiple supported sampling rates  and two channels for stereo sound
3 ready-made drivers from the manufacturer

Alexander

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

We tried all the 8 pwms,but we faced the same issue.

while playing : aplay a2002011001-e02-8kHz.wav
Playing WAVE 'a2002011001-e02-8kHz.wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo
Some sound coming but its not actual .wav file,full noise is coming.

Can you please help to resolve this issue.

Thanks & Regards,

Sankar.  

0 Kudos
Reply

4,426 Views
Sasamy
Contributor IV

Hi Sankar.

We use a third-order RC filter with a 4kHz band without an amplifier.

sk-imx6ull-mb.png

Alexander

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

We implemented above circuit on general perpose board.

 while playing : aplay a2002011001-e02-8kHz.wav 

nothing is coming out from speaker.

on oscilloscope monitor that on c5 one end puls signal is clipping(we are getting before R14 8KHz)

Thanks & Regards,

Sankar

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

We are waiting for your suggestion..

Thanks & Regards,

Sankar. 

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

If we are using wrong amplifier,can you please suggest any pwm power amplifier for playing .wav and mp3.

Thanks & Regards,

Sankar.

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

Now aplay: pcm_write:2004: write error: Input/output error is solved.

But while playing .wav file some disturbance is coming (not able to listen).

We are using attached schematic for pwm audio.

It is correct or con you suggest any example schematic for pwm audio.

pwm_schematic.png

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

I got  logs like below 

root@phyboard-segin-imx6ul-2:~# dmesg | grep "ALSA" -A 3
[ 2.363591] ALSA device list:
[ 2.366577] #0: imx PWM audio
[ 2.384447] EXT4-fs: Warning: mounting with data=journal disables delayed allocation and O_DIRECT support!
[ 2.394270] EXT4-fs (mmcblk0p2): mounting ext3 file system using the ext4 subsystem
root@phyboard-segin-imx6ul-2:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: imxsndpwm [imx-snd-pwm], device 0: snd_pwm_imx [imx-snd-pwm DAC]
Subdevices: 1/1
Subdevice #0: subdevice #0

But whilew playing .wav file i got some Input/output error like below.

root@phyboard-segin-imx6ul-2:~# aplay test.wav -vvv
Playing WAVE 'test.wav' : Unsigned 8 bit, Rate 8000 Hz, Mono
Plug PCM: Hardware PCM card 0 'imx-snd-pwm' device 0 subdevice 0
Its setup is:
stream : PLAYBACK
access : RW_INTERLEAVED
format : U8
subformat : STD
channels : 1
rate : 8000
exact rate : 8000 (8000/1)
msbits : 8
buffer_size : 4000
period_size : 1000
period_time : 125000
tstamp_mode : NONE
tstamp_type : MONOTONIC
period_step : 1
avail_min : 1000
period_event : 0
start_threshold : 4000
stop_threshold : 4000
silence_threshold: 0
silence_size : 0
boundary : 2097152000
appl_ptr : 0
hw_ptr : 0
Max peak (1000 samples): 0x00000018 #### 18%
Max peak (1000 samples): 0x00000038 ######### 43%
Max peak (1000 samples): 0x0000002c ####### 34%
Max peak (1000 samples): 0x00000041 ########### 50%
Max peak (2 samples): 0x00000021 ###### 25%
aplay: pcm_write:2004: write error: Input/output error

Can you help me where i am wrong?

Thanks & Regards,

Sankar.

0 Kudos
Reply

4,426 Views
sankarsalla
Contributor II

Hi Alexander,

Thanks for reply.

This driver will work for imx6ul ?

we are using pwm3 for audio,please find my devicetree file

&pwm3 {
compatible = "fsl,imx-snd-pwm";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm3>;
clocks = <&clks IMX6UL_CLK_PWM3>,
<&clks IMX6UL_CLK_PWM3>;
status = "okay";
};

Is it okay or i have to modify ?

 

can you please provide some examples to test the pwm audio.

Thanks & Regards,

Sankar.

0 Kudos
Reply

4,426 Views
Sasamy
Contributor IV

Hi Sankar.

We use this driver on imx6ull but it should work and for imx6ul, devicetree looks correct.
First, you need to check that the device is in the list of devices for audio playback (in my example the driver is statically linked)

# dmesg | grep "ALSA" -A 3
ALSA device list:
#0: imx PWM audio
random: fast init done
EXT4-fs (mmcblk1p1): INFO: recovery required on readonly filesystem

# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: imxsndpwm [imx-snd-pwm], device 0: snd_pwm_imx [imx-snd-pwm DAC]
Subdevices: 1/1
Subdevice #0: subdevice #0

now you can use any sound player

wget http://www.music.helsinki.fi/tmt/opetus/uusmedia/esim/a2002011001-e02-8kHz.wav -O - | aplay

Connecting to www.music.helsinki.fi (128.214.222.15:80)
Playing WAVE 'stdin' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo
-                    100% |*******************************|  1697k  0:00:00 ETA

mplayer http://www.music.helsinki.fi/tmt/opetus/uusmedia/esim/a2002011001-e02-128k.mp3

MPlayer 1.3.0-6.3.1 (C) 2000-2016 MPlayer Team

Playing http://www.music.helsinki.fi/tmt/opetus/uusmedia/esim/a2002011001-e02-128k.mp3.
Resolving www.music.helsinki.fi for AF_INET...
Connecting to server www.music.helsinki.fi[128.214.222.15]: 80...

Cache size set to 320 KBytes
Cache fill:  8.85% (28993 bytes)   
Resolving www.music.helsinki.fi for AF_INET...

Cache empty, consider increasing -cache and/or -cache-min. [performance issue]
Connecting to server www.music.helsinki.fi[128.214.222.15]: 80...
Resolving www.music.helsinki.fi for AF_INET...
Cache empty, consider increasing -cache and/or -cache-min. [performance issue]
Connecting to server www.music.helsinki.fi[128.214.222.15]: 80...
Audio only file format detected.
Clip info:
 Title: J.S.Bach: Partita E major, Gav
 Artist: Sirkka V�is�nen, vl.
 Album:
 Year:
 Comment:
 Genre: Unknown
==========================================================================
Opening audio decoder: [ffmpeg] FFmpeg/libavcodec audio decoders
libavcodec version 57.24.102 (internal)
AUDIO: 44100 Hz, 2 ch, floatle, 128.0 kbit/4.54% (ratio: 16000->352800)
Selected audio codec: [ffmp3float] afm: ffmpeg (FFmpeg MPEG layer-3 audio)
==========================================================================
AO: [oss] 44100Hz 2ch s16le (2 bytes per sample)
Video: no video
Starting playback...
A:  53.7 (53.6) of 54.0 (54.0)  8.5% 0% $<50>


Exiting... (End of file)

Alexander

0 Kudos
Reply

4,426 Views
Sasamy
Contributor IV

Hello,

there is an ALSA driver for playing any sound

GitHub - sasamy/imx-snd-pwm: A simple sound card based on PWM for i.mx6x processors 

Alexander

0 Kudos
Reply

4,426 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sankar

as suggests "pwm-beeper", seems only monotonous sound "beep" can

be achieved with that driver. For sound recommended to use MQS module,

available for example in i.MX6UL.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply