PMIC for i.MX8QXP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,714件の閲覧回数
shyam_j
Contributor I

Hi,

I am referring to i.MX 8QXP MEK schematics in which they have employed 'PC33PF8100CCES' PMIC to power the i.MX 8QXP processor. In this regard can you please confirm the following:

1) I couldn't find 'PC33PF8100CCES' part on NXP website. Instead there are equivalent parts MC33PF8100FJES/MC33PF8200DEES. Are these the replacement parts for the 'PC33PF8100CCES'? Can you also please confirm the difference between 'PC33PF8100CCES' and its equivalent parts.

2) SW3 and SW4 channels of PMIC 'PC33PF8100CCES' in i.MX 8QXP MEK schematics are powering the VCC_GPU and VCC_CPU respectively. If MC33PF8100FJES/MC33PF8200DEES are replacement parts then SW3 and SW4 of new parts cannot be used to power VCC_GPU and VCC_CPU because the OTP configuration reports for these ICs mention that SW3 and SW4 are disabled. Can you please help us in understanding this conflict/ambiguity?

Regards,

Shyam

ラベル(1)
0 件の賞賛
返信
1 解決策
1,487件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shyam

differencies are described in datasheet

https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf 

MC33PF8100FJES is replacement part for the 'PC33PF8100CCES'.

SW3,4 are disabled for power-up sequence and can be enabled by software

after processor powered up. Note in i.MX8QXP/QM SCU (M4) module is

used for initial starting up of processor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
1,487件の閲覧回数
月泉飞星
Contributor I

igorpadykov

Hi igor

Before the system is downloaded, does M4 automatically turn on SW3 and SW4 after power on? If not,how to control M4 to enable SW3 and SW4 ?

 

Cheers

0 件の賞賛
返信
1,488件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shyam

differencies are described in datasheet

https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf 

MC33PF8100FJES is replacement part for the 'PC33PF8100CCES'.

SW3,4 are disabled for power-up sequence and can be enabled by software

after processor powered up. Note in i.MX8QXP/QM SCU (M4) module is

used for initial starting up of processor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

907件の閲覧回数
Shivam1
Contributor II

Hi igor

Before the system is downloaded, does M4 automatically turn on SW3 and SW4 after power on? If not,how to control M4 to enable SW3 and SW4 ?

0 件の賞賛
返信