PMIC_STBY_REQ holding system in standby on power up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PMIC_STBY_REQ holding system in standby on power up

2,314 次查看
xray
Contributor III

We have a board with an imx6Q CPU that is powered by the MMPF0100 PMIC. 

In normal operation when you power the PMIC (apply a voltage on VIN) VSNVS comes up. PMIC_STBY_REQ (generated by the imx6) comes up at the same time as VSNVS, then after 20 milliseconds PMIC_STBY_REQ drops and the PMIC brings up the rest of it's supplies and the imx6 boots.

Occasionally we've observed the PMIC failing to start.  We traced the behavior to PMIC_STBY_REQ not droping after 20 milliseconds.  Instead it stays high and holds the PMIC in a standby state. 

What could cause PMIC_STBY_REQ to stay high before the CPU boots?  The reference manual shows that PMIC_STBY_REQ is generated by the Clock Controller Module (CCM) but  I don't understand what the CCM does on initial power up (just VSNVS power) and what needs to happen before it drives PMIC_STBY_REQ low.

标签 (2)
标记 (4)
0 项奖励
回复
1 回复

1,131 次查看
igorpadykov
NXP Employee
NXP Employee

Hi j b

this may be caused by incorrect power up sequence

(so some modules not reset properly), for example repetitive

on-off-on-off.. without sufficient pause, so processor

voltages do not fall zero before next power-up.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复