Hi, I am making design based on i.MX6D and I have used PMIC as MMPF0100A. As per datasheet of MMPF0100A, it shows Vin range between 2.8V to 4.5V for 14 Output (Switchers and LDOs). What will be the output voltage of all Switcher and LDOs, if the Vin is below 2.8V? What will be the output voltage of all Switcher and LDOs, if the Vin is below 3.0V? Regards, Mrudang
解決済! 解決策の投稿を見る。
Hi Mrudang
when Vin is below 2.8V output voltage will follow input provided conditions
mentioned in MMPF0100 Datasheet Table 63. SW2 Electrical Characteristics :
Footnote 46. "When output is set to > 2.6 V the output will follow the input down when VIN gets near 2.8 V."
and Table 104. VGEN3 Electrical Characteristics
Footnote 63. "When the LDO Output voltage is set above 2.6 V, the minimum
allowed input voltage needs to be at least the output voltage plus 0.25 V, for proper
regulation due to the dropout voltage generated through the internal LDO transistor."
http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf
That is for normal operation switcher should has 0.2V and LDO 0.25V difference
between input and output voltages
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Mrudang
when Vin is below 2.8V output voltage will follow input provided conditions
mentioned in MMPF0100 Datasheet Table 63. SW2 Electrical Characteristics :
Footnote 46. "When output is set to > 2.6 V the output will follow the input down when VIN gets near 2.8 V."
and Table 104. VGEN3 Electrical Characteristics
Footnote 63. "When the LDO Output voltage is set above 2.6 V, the minimum
allowed input voltage needs to be at least the output voltage plus 0.25 V, for proper
regulation due to the dropout voltage generated through the internal LDO transistor."
http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf
That is for normal operation switcher should has 0.2V and LDO 0.25V difference
between input and output voltages
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
What will be the output voltage of all Switchers and all LDOs, if the Vin =2.8V, 3.0V and 3.3V?
Regards,
Mrudang
Hi Igor,
Thanks for your reply.
As you said "That is for normal operation switcher should has 0.2V and LDO 0.25V difference between input and output voltages".
Does it applicable for all 6 Switcher and 6 LDO Output of PMIC?
Regards,
Mrudang
Hi Mrudang
yes for all
Best regards
igor