Hi,
We are developping a board based on Imx6SXSabresd.
I downloaded Freescale bsp and followed "i.MX_6_BSP_Porting_Guide.pdf" and "Freescale_Yocto_Project_User's_Guide.pdf".
I get the sources with "repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga".
My custom board use the freescale PMIC PF3000.
In this sources i donc find PF3000 support in the device tree.
How can i proceed to use this PMIC?
Does i need to download Fsl community BSP instead?
Thanks a lot,
解決済! 解決策の投稿を見る。
Hi Florian
please look at attached patches.
I am afraid there is support for Imx6SXSabresd with PF3000
in BSP. For other processors one can look example at
linux/imx7d-sdb.dts at master · torvalds/linux · GitHub
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Today we are developping a new board using the last BSP : imx-yocto-L4.14.78.
Is it possible to get the new patchs to apply to support PF3000 on Imx6SXSabresd ?
Best regards,
Florian
Hi Florian
please look at attached patches.
I am afraid there is support for Imx6SXSabresd with PF3000
in BSP. For other processors one can look example at
linux/imx7d-sdb.dts at master · torvalds/linux · GitHub
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------