PF0100 Default configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0100 Default configuration

Jump to solution
1,392 Views
abhijit_mote
Contributor I

1. In default mode of PF0100 there is no mention about the following supplies:

SWBST_VOLT, VGEN1_VOLT and VGEN3_VOLT. Does it mean that these supplies are not enabled?

2. Default configuration of register SWBSTCTL as per data sheet says the SWBST_VOLT is configured as 'ON' and configured for 5.0V.

3. For LDO's there are 4 bits (3:0) for output setting marked as VGENx (Register VGENxCTL) and its default value is mentioned as 0x80. The maximum value 4 bits can achieve is 0x0F. Is this a typing mistake? 

Refer the attachment below for more details.

Tags (1)
0 Kudos
Reply
1 Solution
1,152 Views
art
NXP Employee
NXP Employee

1. The SWBST, VGEN1 and VGEN3 supplies are by default Off in the Default power-on configuration.

2. There is no single reset configuration for supply control registers, it depends on the power-on configuration selected.

3. This is just a typo. Of course, the value of 0x8 is meant.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,153 Views
art
NXP Employee
NXP Employee

1. The SWBST, VGEN1 and VGEN3 supplies are by default Off in the Default power-on configuration.

2. There is no single reset configuration for supply control registers, it depends on the power-on configuration selected.

3. This is just a typo. Of course, the value of 0x8 is meant.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply