PEG Lite (libpeg.a) for Linux (X11)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PEG Lite (libpeg.a) for Linux (X11)

1,341 Views
zafirul_hassan
Contributor I

Hi,

Need libpeg.a compiled for the Linux or can anybody provide link Source Code. How to get the source code for PEG Lite.

With Regards

Zafirul Hassan

0 Kudos
Reply
5 Replies

1,334 Views
zafirul_hassan
Contributor I

We are using iMx8MM, but need linux based libpeg.a for POC

0 Kudos
Reply

1,330 Views
joanxie
NXP TechSupport
NXP TechSupport

unfortunately current bsp doesn't support X11 for imx8mm, if you must use this, you need refer to the bsp for imx6, then porting by yourself, but let me remind, bsp 5.4 doesn't support x11 for imx6 either, you need to refer older bsp version

 

0 Kudos
Reply

1,327 Views
zafirul_hassan
Contributor I

Thanks joanxie,

     Will try the older version BSP and refer iMx6 for reference.

Need one more information it would be help if you could direct me to link from where i can download the PEG for Linux.

As per the Release notes PEG Release Notes

1.2 Special Instructions
         1.2.1 Installation Instructions
         PEG may be installed under Windows as well as under Linux/X11. Following are installation
         instructions for the different platforms.
Windows
         Run the self-extracting PEG installer application and proceed according to the on-screen
instructions.
Linux
        Extract the compressed archive to your preferred working directory and run the installer application following the on-screen instructions.

Can you please provide the link from where I can download the PEG for Linux 

0 Kudos
Reply

1,168 Views
joanxie
NXP TechSupport
NXP TechSupport

maybe you can refer to the PEG link as below:

"https://www.nxp.com/design/software/embedded-software/peg-graphics-software:PEG-HOME"

this is for reference of libjpeg source code

"http://libjpeg.sourceforge.net/"

0 Kudos
Reply

1,336 Views
joanxie
NXP TechSupport
NXP TechSupport

what board are you using

 

0 Kudos
Reply