Hey all,
I need to know which NXP MCUs/MPUs supports more then one Virtual Channel (VC) for PCIe.
I need to realize isochronous data transfers over PCIe.
Thanks in advance!
Hi Julian
virtual channels are supported, for example this is described in
sect.48.2.4 Configuration-Dependent Module (CDM)
i.MX 6Dual/6Quad Applications Processor Reference Manual
or sect.19.2.1.2 Features
i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor!
Maybe I'm blind but in both documents I can't find any answer about how many VC's are supported?
Furthermore I'm quite new in the PCIe-technology and I have a general question:
I want to connect several PCIe-endpoints via a PCIe-switch and the communication between the endpoints must be isochronous.
Is it true, that for isochronous data transfers I need more then one VC also in the endpoints?
Or are the several VCs only for the PCIe switch required?
Hi dav1,
It turns out that you need the VC-capability for all connected PCIe-parts in the system. So while the enumeration phase, the RC will scan the capabilities of each part/port, and when the Endpoint has only one VC, the hole communication path between RC/Switch/EP will only use one VC, even if the switch itself has more than one VC.
For me it doesn't make sense - but that's the way it works...
In the end we kicked all VC/TC-schemes for our system. It is very less supported by manufactures, especially for EPs.
We're going the way to only have realtime/isochronous data in our system. Thus, we won't have to seperate these data streams via VC/TC anymore.