PCIe Endpoint Doorbell or Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe Endpoint Doorbell or Interrupt

5,614件の閲覧回数
carlpii
Contributor I

It is common for a PCIe add-in card to have a "doorbell" register or similar functionality (eg, a queue tail pointer) that the host system can write to start an I/O operation.  I haven't found a way to trigger an ARM interrupt as a result of an inbound PCIe write transaction with the i.MX6 operating in endpoint mode.  I'm currently stuck polling on memory locations which is a really ugly solution.  Is there a way to implement this type of behavior that doesn't rely on polling?

Thanks,

-Carl

0 件の賞賛
返信
1 返信

3,445件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,


The following discussion - hope - helps.

https://community.nxp.com/t5/i-MX-Processors/Endpoint-Interrupt-via-PCIe/m-p/250595

 

Regards,
Yuri.

 

0 件の賞賛
返信