Hello,
We assembled a large number of CPUs on our cards and in about 5% of them the PCI Express PLL cannot lock.
The issue can be solved by raising the 1.0V LDO to about 1.05V in part of the CPUs (this is the maximum working condition). And in part of them the voltage should be raised to 1.1V for PLL lock.
Is this a known issue?
Thank you.
Hi Leonid
reason may be board noise, please check that C458 & C459 are removed.
Schematics (2)
Design files for i.MX 7Dual (REV D)
Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual (REV D)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...
also one can check
PCIe link doesn't come up with XIO2001 PCI bridge on iMX6Q custom board
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Yes the capacitors are replaced with 0R resistors.
The issue is that the initialization process fails before accessing the RESET GPIO pins.
The function that fails is:
static void pci_imx_phy_pll_locked(struct imx6_pcie *imx6_pcie){
u32 val;
int count = 20000;while (count--) {
regmap_read(imx6_pcie->iomuxc_gpr, IOMUXC_GPR22, &val);
if (val & BIT(31))
break;
udelay(10);
if (count == 0)
pr_info("pcie phy pll can't be locked.\n");
}
}
We inspected the voltage on pins AA9, AA10, AA11, AA12 it seems to be ok.
The problem is very consistent on part of the boards:
static void imx6_pcie_init_phy(struct pcie_port *pp){
int ret;
struct imx6_pcie *imx6_pcie = to_imx6_pcie(pp);if (is_imx7d_pcie(imx6_pcie)) {
/* Enable PCIe PHY 1P0D */
regulator_set_voltage(imx6_pcie->pcie_phy_regulator,1000000, 1000000);
ret = regulator_enable(imx6_pcie->pcie_phy_regulator);
if (ret)
dev_err(pp->dev, "failed to enable pcie regulator.\n");/* pcie phy ref clock select; 1? internal pll : external osc */
regmap_update_bits(imx6_pcie->iomuxc_gpr, IOMUXC_GPR12,BIT(5), imx6_pcie->phy_refclk ? BIT(5) : 0);
/* get pcie phy out of reset to get correct clock rate */
regmap_update_bits(imx6_pcie->reg_src, 0x2c, BIT(1), 0);
regmap_update_bits(imx6_pcie->reg_src, 0x2c, BIT(2), 0);
regmap_update_bits(imx6_pcie->reg_src, 0x2c, BIT(6), 0);...
If the bold value is changed to 1100000 than all boards are working. But 1.1V is out of spec...
general way for such issues is to follow procedure described in AN5158
PCI Express® Certification Guide for the i.MX 6SoloX
http://www.nxp.com/assets/documents/data/en/application-notes/AN5158.pdf
Best regards
igor