Output capacitors on the MMPF0100NPAZES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output capacitors on the MMPF0100NPAZES

Jump to solution
1,640 Views
electricar
Contributor I

Hello,

is it allowed to replace the recommended 2x22uF and 4x22uF output capacitors from the attached screenshot with 1x47uF and 2x47uF?

Could this lead to instability of the buck converters due to the higher ESR when paralleling less MLCCs? I couldn't find any useful information about the internal compensation on this topic.

The desired replacement capacitor is this one:

Capacitors | details for GCJ32ER70J476KE01# | Murata 

Thank you very much in advance.

Kind regards

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,473 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello electricar ,

  if 47uF-capacitor is GCJ32ER70J476KE01, no problem. you can replace 2x22uF an 4x22uF with 1x47 and 2x47uF.

Regards,

Weidong

View solution in original post

0 Kudos
Reply
2 Replies
1,474 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello electricar ,

  if 47uF-capacitor is GCJ32ER70J476KE01, no problem. you can replace 2x22uF an 4x22uF with 1x47 and 2x47uF.

Regards,

Weidong

0 Kudos
Reply
1,473 Views
electricar
Contributor I

Hello Weidong,

thank you very much!

0 Kudos
Reply