Hi
I am using gstreramer1.0 with imx8 evk board with yocto build system.
I had build a image with gstreamer plugin for that and able to use it with video H264 & audio.
Now, i would like to use Opus encoder and decoder with gstreamer but some how this components are not available in image.
Other Opus components like rtpopuspay , rtpopusdepay are available in image, I have checked it with gst-inspect component.
I try some work around but not able to get it in image.
Can I get any help in this. any help will be helpfull.
Regards,
解決済! 解決策の投稿を見る。
Hello!
Can someone update information for me does IMX8 on Yocto supports opus audio codec on latest build?
Hello!
Can someone update information for me does IMX8 on yocto supports opus audio codec on latest build?
Hi @Anton_K ,
I have enabled Opus enc and dec in yocto image.
Kernel : 5.10, Yocto : Hardknott, Hardware : imx8m mini
You can add below in you local.conf file
PACKAGECONFIG_append_pn-gstreamer1.0-plugins-bad = " opus opusparse "
Thanks for reply, on my side I have:
Yocto Kirkstone, kernel 5.15
And "opus" codec should be enabled on the gstreamer1.0-plugins-base
And option "opusparse" on the gstreamer1.0-plugins-bad
On the image gstreamer inspect shows:
gst-inspect-1.0 |grep opus
libav: avdec_cllc: libav Canopus Lossless Codec decoder
libav: avdec_hq_hqa: libav Canopus HQ/HQA decoder
libav: avdec_hqx: libav Canopus HQX decoder
libav: avdec_opus: libav Opus decoder
libav: avenc_opus: libav Opus encoder
libav: avmux_opus: libav Ogg Opus muxer
opus: opusdec: Opus audio decoder
opus: opusenc: Opus audio encoder
opusparse: opusparse: Opus audio parser
rtp: rtpopusdepay: RTP Opus packet depayloader
rtp: rtpopuspay: RTP Opus payloader
But on the runtime the opus codec doesn't work.
Best regards, Anton
I don't think current image supports this, did you use rtpopuspay successfully?
No, I've not, anyway thanks for reply.
Probably you can help me? Do you know any guide to run gst webrtc on imx8 (audio + video), I mean actually
Thanks for your response.
Can you please elaborate your statement "I don't think current image supports this". ?
Next,
Regarding rtpopuspay, below it the working pipeline on my pc.
gst-launch-1.0 alsasrc device="hw:2,0" ! audioconvert ! audioresample ! opusenc ! rtpopuspay ! queue max-size-bytes=0 max-size-buffers=0 ! udpsink host=[] port=[]
On board (imx8m mini) I have the below plugins.
root@imx8mm-lpddr4-evk:~# gst-inspect-1.0 | grep -i opus
rtp: rtpopusdepay: RTP Opus packet depayloader
rtp: rtpopuspay: RTP Opus payloader
Other plugins related to opus are not there in image.
But without opusenc this pipline will not work and rtpopuspay will not work here. So, How can I get opusenc and opusdec in my image?
And we need opus because we have to use it in webrtc.
Thanks.
I mean that current bsp doesn't support opusenc or opusdec, for webRTC, pls refer to
"https://developer.ridgerun.com/wiki/index.php?title=GstWebRTC_-_Video_Examples_-_iMX8"
I am able to resolve the issue. Thanks for the support.