Operating voltage range of VDD_xxx_CAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Operating voltage range of VDD_xxx_CAP

824 Views
t-iishii
Contributor II

Hi,

Datasheet of each i.MX6 has an Absolute Maximum Ratings for each VDD_xxx_CAP signal.

But it has no operating range for it. Only minimal value is in comment of each VDD_xxx_IN.

  •  LDO Output Set Point (VDD_ARM_CAP) = 1.225 V minimum for operation up to 996MHz.
  • LDO Output Set Point (VDD_ARM_CAP) = 1.150 V minimum for operation up to 792MHz.
  • LDO Output Set Point (VDD_ARM_CAP) = 1.125 V minimum for operation up to 396MHz.
  • VPU ≤ 328 MHz, VDD_SOC and VDD_PU LDO outputs (VDD_SOC_CAP and VDD_PU_CAP) = 1.225 V6 maximum and 1.15 V minimum.

The other hands, another documents and community comment has a different value for VDD_xxx_CAP.

https://community.nxp.com/thread/440329 

Which is a correct answer of the operating range for VDD_xxx_CAP?

Best regards,

Ishii.

Labels (2)
0 Kudos
Reply
2 Replies

560 Views
t-iishii
Contributor II

Hi Yuri,

Thank you for your information.

I will see the datasheet and check Linux driver for the recommended settings if needed.

Best regards,

Ishii

0 Kudos
Reply

560 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Please use the Table, named “Operating Ranges” in the corresponding DataSheets

and footnotes under the Table for allowed voltages ranges.

The maximum VDD_xxx_CAP values may be taken from the Table for the case
“Run mode: LDO bypassed”.

  Note, the recommended settings may be found as Linux CPU frequency working
point settings in the DTS files. Please refer to Chapter 23 [CPU Frequency Scaling
(CPUFREQ) Driver] of i.MX Linux® Reference Manual.

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply