OpenGL application development on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenGL application development on i.MX6

1,147 Views
frankchenmh
Contributor III

Hi,

I want to develop OpenGL application based on i.MX6 L3.0.35 linux BSP. I know there is gpu-viv-bin-mx6q in the BSP release package and I can run the examples successfully. But there is no source code for it.

Could anyone please advise how to start OpenGL application development on i.MX6 linux?

Thanks!

0 Kudos
Reply
2 Replies

994 Views
art
NXP Employee
NXP Employee

Please refer to the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

994 Views
frankchenmh
Contributor III

Hi Artur,

Thanks for your help. This document doesn't tell me how to setup OpenGL development environment on i.MX6 but it may still useful for me. Thanks!

0 Kudos
Reply