OV5640 mipi i2c access error with 3.10.53 kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OV5640 mipi i2c access error with 3.10.53 kernel

1,141件の閲覧回数
jeromegendron
Contributor I

Hi all,

Yesterday I upgraded my kernel from 3.10.17_1.0.0_ga (boundary devices github) to 3.10.53_1.1.0_ga-pass1 (always boundary devices github).

But unfortunately I can't use my OV5640 mipi camera with the newest kernel (it works with the 3.10.17) : I've got an i2c access error :

ov5642_read_reg:write reg error:reg=300a


I made some logs in the imx i2c driver (driver/i2c/busses/i2c-imx.c), and the problem is with the i2c_imx_acked() function, in the beginning of the i2c_imx_write() function.


Is anyone know what is the problem ? With the same board and 3.10.17 kernel it works !

Thank you for your help !

Jerome

タグ(3)
0 件の賞賛
返信
1 返信

594件の閲覧回数
andyclayton
Contributor I

Have you checked the frequency of the Mclk to the camera sensor, it is possible it has changed in the later kernel

0 件の賞賛
返信